text.skipToContent text.skipToNavigation
Manufacturing competence
Fast delivery
Excellent service
EN
Choose your language
Watchlist
Bookmark products
Direct ordering

KIPP clamping levers - the original since 1952

HEINRICH KIPP WERK has stood for manufacturing competence, inventiveness and technical expertise at the highest level for over 100 years. With a passion for innovation and uncompromising quality, KIPP has established itself as a leading manufacturer of clamping levers - internationally known as the original KIPP levers. They combine reliability, stability and versatility in perfection and set standards worldwide.

The possible applications are as diverse as the fields themselves: Be it in machine construction, the automotive industry, medical technology and healthcare, the foodstuff and packaging industries, electro technology, the wood and furniture industries, construction, metal processing - or in numerous other industrial sectors: KIPP levers convince wherever precise solutions and maximum durability are required.

The combination of tradition and progress results in products that create trust and have been valued nationally and internationally for decades.


How KIPP clamping levers work

Clamping levers are used to reliably clamp and fixate workpieces and other components - e.g. on machines or fixtures. A major advantage of the KIPP clamping lever is the tool-free installation and the rapid adjustment possibility, which guarantees maximum flexibility.

The functioning principle is simple and intuitive: When the grip is lifted up, internal toothed rings situated between the grip and insert disengage. The grip can now be freely rotated without the insert rotating with it. When the grip is released, the toothed rings engage again and connect the grip firmly to the insert. When the handle is now rotated, the insert rotates with it so that machine parts, attachments and/or workpieces can be precisely clamped, positioned or released.

Tradition meets innovation - the evolution of KIPP clamping levers

We began in 1919 as a mechanical workshop which produced kitchen appliances. But a true milestone in our company’s history was the development of the first KIPP adjustable handle in 1952. Over the years, an innovative idea developed into a range that today comprises around 27,500 adjustable handles for a wide variety of requirements and applications .

Features and types of KIPP clamping levers

The types of clamping levers in the KIPP range are as varied as the application fields. All models are available as clamping levers with an internal thread and clamping levers with an external thread. They are also characterised by robust fabrication, a high load rating and easy handling - ideal for a wide range of applications in industry and trade.